This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB2ANY: USB2Any - to check the SPI interface

Part Number: USB2ANY


Hello, 

We are using the USB2Any device to connect to a NOR flash via the single SPI.

However, irrespective of whether the target SPI slave is connected or not, we are getting the same response. 

The target slave is powered ON, (The board on which the NOR flash is placed, is powered ON).

Can you please point me to any documentation which describes how to use this or any specific settings is required.

Regards,

Soumya