Part Number: LMH6733
Other Parts Discussed in Thread: LMH6738, OPA3691, OPA3695
Hi Expert,
LMH6733 and LMH6738 are pin to pin solution, but could you also help to confirm if these two parts are BOM to BOM compatible solution ?
Regards,
Mark
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mark,
after reading the sections "Feedback Resistor Selection" of both datasheets the two OPAmp are not fully BOM to BOM compatible for all gains, but look rather similar for very certain gains.
So, a schematic would be helpful to give a more precise answer.
Kai
Well Mark, they look pin compatible but really can't be functionally identical as teh LMH6733 is about 5.5mA/ch and the LMH6738 is more like 11.3mA/ch.
In this time period, we were all doing triple CFA parts for RGB applications, the OPA3691 is perhaps closer to the LMH6733.
Hi Mark,
Will one of Michaels suggestions work for you or is power consumption a concern? Do we need to dig into the circuit a bit as Kai suggested?
Best,
Sam