Dear Team,
Our customer have an OPA(LM393BIDR) issue as below, please help to check if the design is ok.

When DCIN_27V_1 greater than "V+", the pin1 will output "Hi-Z".
When DCIN_27V_1 less than "V+, " the pin1 will output "0".
But we found that some PCBs behave abnormally
Channel 1 : Pin1 (3.205~3.245V)
Channel 2: Pin2 (2.449~2.482V)
Channel 3: Pin3 (2.365~2.43V)

Many Thanks,
Jimmy