Other Parts Discussed in Thread: LOG114
I am looking for answers and suggestions on TI’s LOG114 (Log Amp). LOG114 provides best results when the input is current (for example: photodiode output). However, for my application, we have to use it with voltage source. We would like to monitor the photodiode’s output (pulse) in two ways:
-one goes to LOG114 and its output goes to the DSP for monitoring the integrated power level;
-another one goes to a connector so that the user can connect it to a scope to monitor the pulse output (50MHz Bandwidth required).
I am thinking of converting the current output of the photodiode to voltage (via a transimpedance amp), then split in two ways, one to the LOG114 and another one to another op-amp (low noise, precision op-amp) that will connect to the the external connector.
Do you have any advise on this approach? Are there any application notes about LOG114 used with voltage input? Are there any better parts to recommend for this application?
Teodor