This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA 116 SPI Read question



Hi,

I am trying to use the SPI of this PGA 116 chip and using 18f4550 processor.

I did not design or create the board, I'm just the software guy who has to make it work now.

From the data sheet (p27 table 4), it looks like I can select a channel and gain in the WRITE command

but not in the READ command as the data sheet shows I have to send a byte of zero's followed

by  0x7A.  I guess (don't know) I have to issue the READ (0x7A00) and then I will get a byte indicating some channel

with data.   Then I don't know if I have to keep reading to get all 10 channels or do I have to issue the READ

command for each channel???

I tried to run some code where I selected the chip (low) , send (SPI write) the READ cmd , set chip (high), then 

chip (low), do read but I only get 0xFFFF responses.  There could be a variety issues to sort through but I guess

while I'm trying to debug this and work with the electrical guy, I was hoping someone could at least let me know

how the READ command should work.  For example, is there a way to specify which channel to read?  To me, the

data sheet seems kind of incomplete in describing the protocol in terms of software.  Thanks!!