Other Parts Discussed in Thread: LM324, MSP430F1232
Hi,
to measure the settling time of a multiplexer (CD4051), opamp (LM324) and ADC, I assembled the following circuit. First select the input to ground (CH1) of the multiplexer and then select the entry with 50mV (CH0).
In the oscilloscope see the following signs:
ch2 -> pin 3 of CD4051 (multiplexer)
ch1 -> output of opamp That is connected to an MSP430F1232 channel ADC (10bit ADC,Rs:2Kohm, C:27pF).
The problem I have is that the signal have a great delay.!!!
The data sheet says that the LM324 opamp has a slew rate of 0.5V/uV much less what I'm seeing in the oscilloscope.
What hapened here?
thank,
regard,
(sorry for my the elemental english...)
Mauricio.
this pic is a zoom: