Part Number: TL054
Other Parts Discussed in Thread: TL084, TL084H,
The "TL05x, TL05xA datasheet (Rev. A)" in the "absolute maximum ratings..." section includes Note 3 "The magnitude of the input voltage must never exceed the magnitude of the supply voltage or 15 V, whichever is less" and also includes a specification for "Input current, II (each input) " of +/-1mA. What can happen to the op amp if the magnitude of the input voltage exceeds the supplies but is clamped to limit the current so it never exceeds +/-1mA either when the supplies are power cycling or when they have reached their steady-state values?
The TL084 also includes the same note "The magnitude of the input voltage must never exceed the magnitude of the supply voltage...", but does not include a maximum input current specification (but TL084H does include a note that "Input pins are diode-clamped to the power-supply rails. Input signals that may swing more than 0.5 V beyond the supply rails must be
current limited to 10 mA or less.").
What can happen to the TL08x-non-H-suffixed devices if the input Voltage exceeds the supply voltage even if the current is limited to +/-1mA? Would the internal ESD-protection circuitry divert the current to protect the op amp?