Part Number: OPA376
Hello support team,
I am working on a differential circuit with the OPA376AID which interfaces between a current sensor and an ADC and I do not have the expected behavior of the differential circuit.
Here is the circuit:
R1=R2=R=10K
R3=R4=R'=80K
Vout=(V2-V1)(R'/R)

Input:
V1 = 1.65V
V2 = 1.65V
Theoretically I should have Vout ≈ 0 V, which is confirmed by the simulation on LTspice.
This is what I'm measuring :
Vout = V2 = 1.65 V, I have the behavior of a voltage follower, Indeed I have always Vout = V2 ...
Do you have an explanation ?
Please correct them if there is a mistake.
Best regards,
Constant