Hi there,
I have an application that runs on less than 1mA, therefore my planned design is as above. Three areas of concern/uncertainties arise and are:
1) To minimize quiescent current, can I set R1 & R2 to the values as shown above? The datasheet states that the maximum Input Bias current is 15nA, therefore 1 Mega-Ohm should not pose any problem as it is still >50 times smaller than the expected input impedance into the INA200's comparator. Am I right in the interpretation of this specification?
2) The Comparator's output is rated at 18 Volt Max, but the datasheet says this can be exceeded provided the current is kept below 5mA. My circuit has effectively 20 kilo-ohm to 40V, resulting in 2mA of current and therefore within the clause, but surely all transistors/FET's have a breakdown Voltage, therefore what is the actual breakdown Voltage and if it is indeed exceeded with the current limit in-place, will the circuit still function correctly or will it be in an undefined/latch-up state?
3) As for my reset, I like to have an additional 4 second delay (in hardware), hence the 1uF capacitor added to the reset input and relying on the internal 2 Mega-Ohm as my discharge resistor to set a rough time constant (accuracy is not a concern). Can the reset input handle such a slow voltage decay on its input or will it behave unpredictable? i.e. is it a Schmitt trigger type of Input with its low threshold at about 1.1V or is it some other circuit that will go into a "linear" region with potentially "bad" behavior? Section 7.3.3. in the datasheet does not give any detailed rationale behind the RC circuit nor on maximum limit of the capacitor that is allowed to be used in the RC Filter. I will be driving it with 5V and after removing the 5V (Same as on V+ of the INA200), I want an additional 4 second delay (approximate). Mine is not a case of driving it with a different voltage than V+ for which section 7.3.3 seems to try and address.
Regards
Thomas