This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV1702: TLV1702AIDGKR

Part Number: TLV1702


Hello,

We received PCN 20220512000.1 which brought up some questions, in particular about P/N TLV1702AIDGKR. 

Can you please confirm if part TLV1702AIDGKR currently has NiPdAu or NiPdAuAg terminal finish? Which (NiPdAu or NiPdAuAg) has always been the terminal finish of this part? After August 12, 2022, the part will ship as (Matte Sn or NiPdAu), (Matte Sn or NiPdAuAg), or (Matte Sn or NiPdAu or NiPdAuAg)?

This information is important to us because based on TI’s Pd, Au, Au-Ag terminal finish thicknesses, our lead free control plan may or may not require hot solder dip, depending on the NiPdAu and NiPdAuAg terminal finish. We need to know how to disposition future parts. 

Additionally, can you please clarify which of the statements below is the correct interpretation of PCN 20220512000.1?

1. Parts listed in the PCN that originally had NiPdAu finish will be shipped with either NiPdAu or Matte Sn finish, under the standard part number. Those with originally NiPdAuAg finish will be shipped with either NiPdAuAg or Matte Sn finish, under the standard part number .

2. All affected parts in the PCN will be shipped with either NiPdAu, NiPdAuAg, or Matte Sn, under the standard part number.

3. All affected parts in the PCN will be shipped with NiPdAuAg or Matte Sn under the standard part number and only those with G4 suffix will be NiPdAu.

Thanks,

Jasmine

  • I'd like to add another sentence to the possible interpretation of PCN 20220512000.1 to clarify. Please confirm which is the correct interpretation:

    1. Parts listed in the PCN that originally had NiPdAu finish will be shipped with either NiPdAu or Matte Sn finish, under the standard part number. Those with originally NiPdAuAg finish will be shipped with either NiPdAuAg or Matte Sn finish, under the standard part number. And those with G4 suffix will be NiPdAu finish only.

    or

    2. All affected parts in the PCN will be shipped with either NiPdAu, NiPdAuAg, or Matte Sn, under the standard part number. And those with G4 suffix will be NiPdAu finish only.

    or

    3. All affected parts in the PCN will be shipped with NiPdAuAg or Matte Sn under the standard part number and only those with G4 suffix will be NiPdAu finsih.

  • Hello Jasmine,

    I have forwarded your question internally to get a more authoritative answer. This is rather specific and may take a day or two to fully answer.

  • Hello Jasmine. Please see answers below. Answers in red:

    Can you please confirm if part TLV1702AIDGKR currently has NiPdAu or NiPdAuAg terminal finish? NiPdAuAg

    Which (NiPdAu or NiPdAuAg) has always been the terminal finish of this part? NiPdAuAg

    After August 12, 2022, the part will ship as (Matte Sn or NiPdAu), (Matte Sn or NiPdAuAg), or (Matte Sn or NiPdAu or NiPdAuAg)?  Matte Sn or NiPdAu or NiPdAuAg

    Additionally, can you please clarify which of the statements below is the correct interpretation of PCN 20220512000.1?

    2. All affected parts in the PCN will be shipped with either NiPdAu, NiPdAuAg, or Matte Sn, under the standard part number.  This one is the correct interpretation.