Part Number: TLV170
Other Parts Discussed in Thread: TLV9101, TLV9301,
Hello,
I'm working on an upgrade to an analog front end in a product and I would like to take a data acquisition input channel from fixed Fc to a configurable Fc via MCU. I've been reviewing the sallen-key and multi-feedback topologies (I'm using the sallen key now) and have run into a problem with both topologies.
Using the following two articles (sallen key and multi-feedback App notes):
They both indicate that the Q value of the filter is tied to the Fc by way of the resistor and caps. It seems that the corner frequency is tuned by some of the same passive components the Q values are tuned with. This means I can't adjust the corner frequency of the filter without affecting the Q value. This is a problem because I want the Q value to stay at 0.707 so I don't have excessive attenuation or peaking which could cause overshoot on fast edge rates.
Is it possible to use one of these topologies or a different topology to design a filter supporting a configurable Fc while keeping the Q the same value? I was planning on using a digital POT to modify the resistors for different Fc values, but now I see doing this will cause the Q to change every time I adjust the Fc of the filter. At this point I think I've gone down a fundamentally incorrect path.
Thanks for any input!