This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2277: OPA2277U

Part Number: OPA2277

Hello

PN: OPA2277U

What shall be the maximum allowed reflow cycles of OPA2277U?

What shall be the impact on the reliability if we will exceed the maximum allowed reflow cycles?

thank you

  • Hi Ruby,

    this docmunent says that the IC packages can withstand three reflow cycles:

    6622.spraby1a.pdf

    Keep in mind that soldering counts to the most stressful events in the life of a chip. So, the number of reflow cycles should be limited to the absolute minimum. This is especially true for a high reliability application.

    The internals of chip are sealed by the epoxy package material where the pins come out of the package. Soldering stress can result in a delamination at this point and the die will no longer be fully sealed against moisture afterwards which can result in internal corrosion and premature failure. But long before this destruction the die becomes sensitive to moisture and some of the electrcial specifications may no longer be valid.

    Kai

  • Hi Ruby,

    The document that Kai references is TI's official statement on the reflow subject.

    Unofficially we have taken some Precision Amplifiers devices out to 5 cycles and the product remained robust. That was an unofficial experiment and we neither provide the data, or make any assurance beyond the 3 cycles referenced in the SPRABY1A Applications Note. All risk is assumed by the customer for application of more than 3 cycles.

    Regards, Thomas

    Precision Amplifiers Applications Engineering