This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BUF634A: Capacitive load and TINA TI SPICE MODEL

Part Number: BUF634A
Other Parts Discussed in Thread: LMH6321, , BUF634, TINA-TI

Hello,

We have compared the performance of two IC buffers: BUF634A and LMH6321 to drive a large capacitive load (e.g., 1nF) using a very simple circuit. Simulation results based on the free Tina TI software indicate that LMH6321 shows a better transient response than BUF634A. Is the free TINA-TI using the right BUF634 spice model? From older posts, it seems that the model implements the wide-bandwidth mode.

Thanks,

Enrique

PS: Test circuit consists of the source (square wave) directly connected to the buffer. The ouput of the buffer is connected to the capacitive load.