Part Number: LMV604
Other Parts Discussed in Thread: TLV9004, TLV2464, TLV2784, OPA4342, OPA4316
Number: CS1215541
Contact: David Heyl
First name: David
Last name: Heyl
Short description: Output goes non-linear at upper end of range
Phone: 15137775233
Email: dave.heyl@pe-ltd.com
Company: Performance Electronics
Company phone:
Language: English
State: Open
Provide case details or comments:
I specified the LMV604 as an alternate for an MCP6L04 op-amp that we couldn't acquire - these op-amps are used on a large number of our products. We now have the first batch of boards moving through production and boards with the LMV604 are failing our production test. The test is fairly straightforward - we input 0V, 2.5V, and 5V, and then check the output from the op-amp within a range. The circuit is simple (shown at bottom) - an RC at the input and then a voltage divider to reduce the input down to a range of 0 to 3.3V since the op-amp is powered from a 3.3V supply. When I did more detailed testing with the LMV604, the output jumps to the rail somewhere around a 4.7V input as shown below. The MCP6L04 op-amp in the same circuit is linear all the way to the rail, as shown in the second illustration below. Can you explain this? How would I have pre-determined this issue from the datasheet when I was selecting alternates? This was completely unexpected. When I was checking parameters relevant to this application, I saw that this is a rail-to-rail output. And it does go to the rail, but not in a way that is useful, in my opinion.