Other Parts Discussed in Thread: INA282, INA285, INA212, INA193
Dear all,
I need your assistant for choosing the correct high side current sensing amplifier.
Specification:
1) need to sense the current in both the directions ( +20 mA to -20mA)
2) current sensing resistor is as low as possible.
I found INA282 is one which has 70uV offset voltage. The inbuilt gain is low (50V/V).
I think INA285 is suitable for my application. It has inbuit gain of 1000V/V.
Calculations:
INA285 Specifications
Gain = 1000;
Vsupply = 5V
Vref = Vsupply/2
min current = -20mA
Max current = 20mA
Vsensemax = (Vsupply-0.4-Vref)/Gain
Vsensemax = 2.1mV
Rsensemax = Vsensemax / maxcurrent
Rsensemax = 105mOhm
Is this current sensing amplifier(INA285) is in production?
Is there any amplifier that will provide bi-directional current sensing with high gain then we can use very low current sensing resistor (~10mOhm)?
Please provide your comments on this application.
Thanks
Regards
Ram