Part Number: INA186
Other Parts Discussed in Thread: RCV420
I am looking to build a 4-20mA to 0-3.3V conversion circuit. The 4-20 mA input is generated by loop powered / externally powered (24V) process control transmitters (eg https://rishabh.co.in/uploads/product/Datasheet_-_CT_with_inbuilt_Transducer_Ver_C1.pdf page 4). The 0-3.3V output is to be interfaced to ADCs. I was thinking about RCV420 or INA186 based solution (4-20mA goes through a shunt R -> this is fed to the input of INA186) and I liked the block diagram on the first page of INA186 datasheet - it looks very clean and does not have the thermal drift problems associated with RCV420. However I am a bit hesitant to use the circuit as shown on the datasheet because there is no isolation between the 24V from the sensor and 3.3V from my microcontroller. Can you suggest any alternate solution than can do 4-20 mA to 3.3V conversion, but also provides isolation ?
Thanks.