Part Number: LF198QML


The Pin-5(output) value was expected to be output to almost '0V' level according to Pin-3(Input), but it was confirmed that an unspecified value (about 1.6V) was output upon the start of the +15V supply voltage input. (Refer to the green box in the measured waveform picture.)
If Pin-7(Logic ref.) is entering High(5V) before +15V supply voltage is entered, please check if it can be output to an unspecified value(about 1.6V) such as Pin-5(output) in the green box of the above waveform picture.
Thanks
best regards.