I've been scratching my head for a bit and cannot seem to find the right path. I need an analog solution that uses minimum IC usage for a circuit that does the following.
* When Vin = 0 to 1.2V, the output remains at 0V
* When the input varies from 1.2V to 5V, the output linearly varies from 0 to 1.5V
* Supply voltage is 7V and ground
* I may have to adjust the 1.2V setting later
I was looking at a rail-to-rail opamp, but cannot get anthing working properly.
My other option is to use a current amp whereby the output current is 0A until I hit the 1.2V input. Then the current ramps up. I have not designed with current opamps yet to really know the right approach for the design.
Any support would be greatly appreciated.
Derek