Part Number: TL072
It was identified in the technical tests of our products, the component TL072 of the manufacturer Texas of the lot 1621012MY1, giving a difference in
value and consequently not functioning properly for the products. It was identified in the tests, that from 4KHz, the product has a significant drop in
response. At 18KHz the result is -8dB on the product.
2,500 pieces were used, and they are also being sent, but outside their encapsulation and with traces of solder.