This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA277: Output short circuit of absolute maximum rating

Part Number: OPA277

Hello,

I am designing op-amp circuit that circuit will use OPA277.

The output short circuit of absolute maximum rating is defined "continuous" on section 6.1 of OPA277 deta sheet.

I would like to confirm the mean of the "continuous".

Does that mean that destruction or deterioration of this device is prevented by the function of a internal protection circuit or the like?

Regards,
MESH

  • Hi Mesh,

    don't overlook the footnote (2) in the "absolute maximum ratings"!

    The short-circuit current is limited to typically 35mA. This current times the supply voltage is the heat dissipation the OPAmp has to handle during a short-circuit. With a +/-15V supply 525mW has to be dissipated during a short-circuit condition, which is quite a lot. With a thermal resistance of 110°C/W of the SOIC package the die will heat up 58K above the ambient temperature.

    Now it becomes clear what "continuous" means: If the ambient temperature is low, the short circuit can last longer. But if the ambient temperature is very high, the short-circuit becomes very stressing for the OPAmp and the short-circuit should not last longer.

    The short-circuit protection of an OPAmp is like a fire extinguisher. It's something for the emergency case, but nothing for repeated or even planned use. If the output can be short-circuited repeatedly during normal operation, add a current limiting resistor in series to the output of OPAmp. This also serves as an isolation resistor isolating the output of OPAmp from destabilizing capacitive loads.

    Kai

  • Hi Mesh-san,

    Does that mean that destruction or deterioration of this device is prevented by the function of a internal protection circuit or the like?

    The table and graph below specified how Continuous in output short-circuit is defined. 

    1. Isc is only defined in one amplifier per package. 

    2. Isc or output short-circuit in continuous is defined within the recommended operating temperature range for a short duration. The IC should withstand the heat dissipation with the short-circuit (not exceeding the maximum junction temperature rating). 

    3. The short-circuit op amp should not be self-destructive due to the event for a short duration. The circuit should be self-recovered and operated normally after the short-circuit current condition is removed. Please also see Kai's comments. 

    If you have additional questions, please let us know. 

    Best,

    Raymond

     

  • Hi Kai,

    Thank you for your reply.

    I understand your reply.

    Regards,

    MESH

  • Hi Raymond,

    Thank you for your reply.

    I will design my circuit reflecting your reply.

    Regards,

    MESH