Part Number: OPA830
Hello,
I'm designing a sallen-key LPF. The output seems has some oscillation, and the oscillation is always near 0V to DC-bias (above is the input signal and below is the filtered signal).


The oscillation is aournd 50MHz, 110mVpp

I know there's high frequency feed through issue with active filters, but I assume if this is the cause, th oscillation shall not be fixed on the same position (or the noise is always keep same phase???).
Anyone who can help explain it? Thanks!
Simulation is shown below: