All,
I need the mechanical info for TI's OPA330 in XBGA (YFF) package. Package dimensions 'D' and 'E' are missing from the datasheet (sbos432e). Any help will be greatly appreciated.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TIguru,
I see that page 36 of the datasheet should not have been included. You're right, we don't have a 25 pin package for the OPA330. Page 37 is more relevant and it still doesn't include the "D" and "E" dimensions.
From http://www.ti.com/sc/docs/psheets/jedec/s_xbga_n.html I was able to find the following information:

I think "D" and"E" are the width and length, respectively.
I will see if I can get the correction in the datasheet.
Regards,
Chris
You're welcome, but unfortunately I just found some addtional conflicting information. Figure 25 in the datasheet gives different numbers:

I will look into this conflict.
Regards,
Chris
TIguru,
Figure 25 in the OPA330 datasheet is correct.
The TI package website dimensions are the max dimension of that package. This type of package is unique that the actual package dimension size varies with the size of the die inside. Therefore, we specify the exact size of the package in the datasheet. Page 37 doesn't show these dimensions since it is a generic diagram that is used for all of the YFF packages.
Best regards,
Chris