Hello,
I want to design a AC current source of current variable up to 30mA rms.
The frequencyrange of the current source should be from 1Hz to 100KHz.
The load is mounted in a nitrogen-flow-cryostat an therfore will change
it's resistance with temperature between 20 and 100Ohms.
The AC input signal originates from a lockin amplifiers Oscillator
output, is referenced ro ground and can be chosen between 0 and 4Vrms. the outputcurrent will be sourced to ground. features of
this current source should be a very low excitation of higher harmonics, low noise, very low offset.
I thought about a howland current source. my questions are: which opamp would be the most adequat choice for my requirements? Is there even a more convinient way of realising such acurrent source?
Thanks.