Other Parts Discussed in Thread: AMC1311, , INA143, INA146, PGA281, PGA280

Hello?
As title, please review for circuit.
Input and Output range of AMC1311 are 0 to +2V.
Gain of first INA326 is 10.(2V to 20V range)
Gain of second INA326 is 0.1.(20V to 2V range)
And then, problem is offset.
Using +1V Refence, if connect to wire like picture, is it possible? (0 to +2V -> -10 to +10V -> 0 to -2V)