Part Number: TLV2172-Q1
Hello Team, my customer has following question:
In the datasheet (SBOS784C –NOVEMBER 2016–REVISED JANUARY 2019), short-circuit current is defined as shown below.
I want to make sure that my understanding is correct, and I was hoping you could help.
In our case, the operational amplifier is configured to output either 5V or 8V5 at Pin1 (with feedback on Pin2). Now, let’s suppose that a short to ground occurs at this pin (OUT A).
Does the definition below mean that the current will be internally limited to 75mA (typical)? If yes, is there timing limitations to this protection feature? Or can this current be applied continuously?

Many Thanks
Josef