Part Number: LMV331
Other Parts Discussed in Thread: TLV9032, TLV7011, TLV7021
Hi team,
what will happen to the output when the power on VCC is not yet 2.5V ?
is there any reset circuit inside that can prevent this unstable phase?
Regards,
Fred
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Fred
Thanks for your post. Unfortunately, devices such as the LMV331 do not include a power on reset circuit. If that is required, may I suggest our TLV7011 (push pull) or TLV7021 (open drain) family of comparators which has a POR circuit. We just do not have enough characterization data on the LMV331 in order to provide a warranted startup condition. Most likely the LMV331 will start high Z at the output but as it reaches the recommended operating range, it is possible that some unpredictable output conditions could occur. If the TLV7011/21 is not fast enough, we will be releasing a single channel variant of the TLV9032/22 family soon and this will also include POR circuit.
Chuck
Hi Sins,
may I know why POR can prevent this?
is there a diagram or picture that can explain this?
thanks
Fred
sorry for the delay. I am not exactly sure what you are looking for but essentially a POR circuit holds the output of the comparator in a known state until the supply reaches the recommended operating voltage. Just think of it as a comparator within the comparator that monitors VCC. When the VCC is below the operating voltage, it holds the output in a known state. Once VCC reaches the operating voltage range, the POR circuit relinquishes control of the output and now the output tracks the input of the comparator.
Chuck