Other Parts Discussed in Thread: AMC1311,
Dear team,
If the VIN-GND1=-0.5V, what is the output behavior? We only list the output behavior when VIN>-0.1V.

Thanks & Best Regards,
Sherry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
If the VIN-GND1=-0.5V, what is the output behavior? We only list the output behavior when VIN>-0.1V.

Thanks & Best Regards,
Sherry
Hi Sherry,
The specified linear range of the AMC1311 is from -0.1V to +2V, so that is why Figure 48 is limited in its negative range.
Hi Sherry,
It's 'undefined' - the outputs will start to clip and will look distorted.
Hi Tom,
Thanks for your reply!
Our device's output will connect to one amplifier's input, and the input's absolute minimum voltage rating is -0.5V. In the customer's system, there is VIN=-0.5V condition for AMC1311-Q1, so we want to know whether the output will exceed -0.5V at this condition/VIN=-0.5V?
Thanks & Best Regards,
Sherry
Hi Sherry,
There is nothing inside the AMC1311 that can drive its output below ground.