This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BUF634A: Spice simulation error

Part Number: BUF634A

Hi,

I was trying to run a spice simulation with the BUF634A high-speed buffer but I get this error.

I imported the BUF634A spice model from the TI webpage.

Thanks in advance,

  • Hello Jerome,

    I have replicated your issue on my device; I am looking into the cause for such a behavior.

    Best,

    Alec

  • Hello Jerome,

    I have the solution: when importing a model into PSPICE, you must ALSO add the .lib library file into the simulation profile when you create a new simulation.

    For example, with the BUF634A zip folder for PSPICE, there is a .lib file called buf634a_a.  This is the library file for the model; the model information is contained in the .OPJ file extension.  In order to add the buf634a_a.lib file to the simulation profile, go to the configuration tab/menu when you are in the create or edit window of the simulation profile:

    Please follow along with these annotated screenshots to add your buf634a_a.lib file to the simulation profile configuration tab.  You may 'add to Global' if you wish, but I usually keep my library files associated with each design.  

    If you have issues or need additional clarity, please reconnect on this thread.

    Best,

    Alec