Other Parts Discussed in Thread: XTR112
Hello. I'm in trouble with a XTR112. I inteded to use it as a variable current generator for simulating a 4-20mA sensor.
It works quite good, except in the near 4 mA zone. I can't get it to regulate smoothly between 4 to 7 mA zone, it changes abruptly from 4.1 to 5.2 mA.
My zone of interest is from 4 to 12 mA.
Any clue ? attached is an image of my implementation. I feed 12VDC in X1. In J3 I have a LED and in J1 I have a 5K linear potentiometer.
Thanks in advance.
Matias, from Neuquén - Argentina