Other Parts Discussed in Thread: OPA861, OPA2670, OPA2673, OPA627
Hello,
I am currently working on a project regarding Visible Light Communication using a LED module at the Tx and a PIN Photodiode at the Rx.
The driving circuit for the Tx consists of the following components: a double-stage TCA topology (OPA861 + Class-AB Current Amp), a Bias-Tee and the LED module itself. I intend to feed the OPA861 with an AC Baseband signal (let's say max 1 Vpp), in order to get a Voltage-amplified AC current signal at its output. The output-current will most possibly be post-amplified by a Class-AB Amp, and further pass through a Bias-Tee being coupled with a constant DC current (700mA), required for powering the LED module.
OPA861's datasheet is referring to "Wideband LED Drivers" under its Applications. Could anyone assist me on the design of this circuit? I mean, have there been any similar applications using the OPA861?
Any help will obviously be highly appreciated! Thank you in advance!
Best Regards,
David