Part Number: OPA593EVM
Other Parts Discussed in Thread: OPA593
Dear Technical Support Team,
Could you share the size of board such as height and width.
If you can provide CAD data(AW), could you provide it?
Best Regards,
ttd
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello ttd,
The approximate dimensions of the OPA593EVM are:
Length 13.4 cm
Width 10.8 cm
Height 3.1 cm
The OPA593EVM PCB layout was created using Altium software and we do have the Gerber files for the board. We don't openly post the files to the e2e because TI can easily lose control of our intellectual property. We can discuss the possible release of the OPA593 EVM Gerber files to you offline if we understand your full intent and use of them.
Please send me an e2e "Friend Request" so that I can receive your email address. We can then further discuss your request.
Regards, Thomas
Precision Amplifiers Applications Engineering