Part Number: AMC3302-Q1
Other Parts Discussed in Thread: ADS131B02-Q1, ADS131B04-Q1, ADS131B26-Q1
We are trying to design an isolated current measurement design based on a shunt measurement principle for high battery charge and discharge currents. The design should feature digital signal transmission to a master MCU, preferably via CAN. The AMC3302-Q1 could be a starting point for the design, but i wondered wether there is a more comprehensive solution to this problem.
With our power loss requirements (see below) the input voltage range of the AMC3302-Q1 is not favorable. We would not be using the full range when using a small shunt resistance (25µR to 35µR), therefore sacrificing resolution.
We would like to meet the following specifications for our measurement:
|
Parameter |
Value |
Unit |
|
Nominal Measurement Range |
±500 |
A |
|
Power Loss (Shunt) |
<9 |
W |
|
Total Accuracy |
±0.4 |
%rdg |
|
Offset |
75 |
mA |
|
Linearity |
0.01 |
% of range |
|
Resolution |
27 |
mA |
Additionally we want to integrate various temperature measurements. Specifications on this still need to be worked out, but it may be relevant to an answer for the current sensing architecture.