This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1311-Q1: max Vos across temperature range

Part Number: AMC1311-Q1

Hi team, 

Could you please share how to evaluate the max Vos across -40~125C for AMC1311B-Q1?

For the +-1.5mV max, it is for 25C. And for 10uV/C TC, it is valid for full temperature range. Is my understanding correct?

if so, can I calculate the worst case Vos across temperature range is -1.5-0.01*(40-(-25)) to 1.5+0.01*(125-25), which is -2.2mV to 2.5mV when VDD1=5V ?

Thanks for your clarification

Scarlett