Part Number: LMH6882EVAL
Over what frequency range does this evaluation board operate? I know the amplifier chip itself can operate between 0-2.4 GHz, but the baluns listed on the schematic/in the pictures (Mini-Circuits JTX-2-10T+) seems to only operate over 0.05-1 GHz and is matched for 75 ohms (and 150 ohms differential) instead of 50 ohms (and 100 ohms differential). Is this the correct balun? If it is, does that mean that the eval board (when used in its default single ended configuration using the baluns) only works under 1 GHz?