This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA454: High voltage OP with lower current consumption

Part Number: OPA454

Dear ,

The customer currently solution is ADA4700, and RD also test TI OPA454. The thermal is higher than ADI

Iq ADA4700 ( TYP): 1.7mA, Iq OPA454  (TYP): 3.2mA

Do we have any solution to replace ADI ADA4700?

Thanks & best regards.