Part Number: TLV9062-Q1
Other Parts Discussed in Thread: TLV9062, OPA2192
Hi Team,
Our customer has some clarifications about the Input Bias Current of the TLV9062 and TLV9062-Q1 as follows.
I am using some TI Op Amps in a high impedance application and I need confirmation on the "Input Bias Current" specification.
I think that there is a mistake (misprint) on the TLV9062-Q1 data sheet. On the first page under "Features" it states "Low input bias current: 0.5 pA". However, on page 8, under "Electrical Characteristics", the "Input Bias Current" is listed as 5 pA. So, which is correct?
Also, on the first page on the TLV9062-Q1 data sheet, it states that the performance specifications are identical to (non-automotive qualified) part TLV9062. This (non-automotive) part has the Input bias current specified as 0.5 pA in both the "features" and "Electrical Specification" sections. I assume that this is the correct value.
There may also be a misprint regarding the "Input Offset Current" on the TLV9062-Q1 data sheet. It's listed as 5 pA, when perhaps it should be 0.05 pA like the TLV9062.
Finally, I'm also using a "higher voltage" Op Amp, the OPA2192. Could you confirm that the "Input Bias Current" and "Input Offset Current" are 5 pA and 2 pA respectively?
In summary, please confirm the values for the "Input Bias Current" and "Input Offset Current" for parts TLV9062-Q1, TLV9062, and OPA2192.
Regards,
Danilo