Part Number: OPA2691
I am designing a high speed amplifier using the OPA2691 in an inverting topology. Upon initial use, the op amp was drawing 100+mA of current on both the positive and negative supplies. The op amp is being supplied with +/- 5V. I was originally seeing on an oscilloscope that the op amp was oscillating with no input connected. After resolving this issue and no longer having the op amp oscillating, the current being drawn was about 60mA. The test bench set up was with no input, no load, and no oscilloscope probes connected (to not have the added capacitance). The datasheet says that quiescent current is 10.2mA. I was wondering if there is anything I am overlooking or any solutions to reduce this amount of current being drawn. Any help would be great, thank you!