This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA240: Output non-linearity / inversion, at frequencies higher than BW

Part Number: INA240


Observing anomalous behaviour on the output of INA240A3 and A2, and grateful for all help and insight.

Sensed current waveforms on the output of the INA240 sporadically appear to be inverted, or significantly reduced in amplitude, compared with adjacent, correctly sensed, waveforms.

Blue: INA240A2 OUT

Green: Voltage measured across 0.1 Ohm resistive load, in series with 300 uOhm current sense resistor

Observe the undershoots in blue of INA output, that do not appear in true current waveform, visible in green.

(The load voltage (/current) increases following an INA output undershoot, as the compensator responds.)

Switch transitions appear to be "skipped" in the output of the INA240, or even a positive triangle inverted into a downward.

Application: high side current sensing for an average-current controlled buck converter.

Supply voltage: 5V from LDO. Decoupled with 2x 100 nF, 1x 1uF

Reference: 500 mV (ADR130AUJZ) decoupled with 100nF + 1 uF.

Half-bridge switching frequency is 1 MHz.

The switching frequency was reduced to 500 kHz, to exceed the INA240 BW by less margin.

Anomalies in output still observed, though now do not appear to be inverted, rather significantly attenuated.

The CM voltage that the IN+/- are exposed to is that represented by the green trace, load voltage.

No noise is observed on the supply or ground corresponding with the sporadic anomalies.

No CM or DIFF filtering has been added to the current sense input.

The target here is not to sense the peaks of the current waveform at the switching frequency, but rather the average current so the gain roll-off at 1 MHz was expected to be acceptable - but the anomalies effect the average.

Grateful for any guidance and advice. Issue has been observed on multiple IC units, and on INA240A3 and A2.

  • Hi Aaron,

    the INA240 is way too slow for your 1MHz application. You cannot run a 400kHz amlifier at 1MHz. It's like using an OPAmp: To have enough linearizing gain reserve your maximum frequency of application should be at least one decade below 400kHz. See figure 8-1 of datasheet. Of course, you can violate this rule but then you have to live with huge errors.

    Kai

  • Hello Aaron, 

    I agree with Kai about the bandwidth.  We have a higher bandwidth device in the INA241 but this may not deal with what you require.  Below is a section on the datasheet from the INA241.  The INA241 is the fastest bi-directional current sense amplifier we have.  You may need to have a low side sense with a high speed amplifier that you will need to deal with voltage transient and voltage input limitations on the high speed amplifier.