This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLE2144: output signal distortion;

Part Number: TLE2144

Hello  Team,

I am currently using a TLE2144IDW, and the input signal of 600 kHz, 4.2Vpp is generated from a function generator.

Using a voltage follower with TLE2144, I was able to get an output of 4.2Vpp with an input from the function generator, but after it reaches above 510 kHz, the signal starts to distort on the negative cycle.

The gain bandwidth of TLE2144 is around 5 MHz, and the slew rate is 27 V/μs. Therefore, I should be getting a good signal on the output, yet the negative cycle of the signal looks slightly distorted. Not sure what the issue is. I do not know what I need to look for.

Schematic:

Dual Supply of +/-12 V

Image shown below (input: cyan signal, output: yellow signal):

 

I hope to hear from you on this. 

Best Regards

James Man