Part Number: INA231
I have two questions.
1. I think the conversion time is determined by the values of VBUSCT2~0 and AVG2~0 in the Configuration Register in Continuous Mode.
If a value is set in the Configuration Register for the first time and the same value is written to the Configuration Register again before the conversion time has passed, will the conversion time start from the access time to the Configuration Register for the second time?
Or, since it is the same value, does the conversion time start from the first access time to the Configuration Register?
I would like to know if the conversion time is cleared each time the Configuration Register is accessed.
2. Is it correct to assume that the various monitor data at addresses 0x01~0x04 will display the previous previous data during the conversion time?
Translated with www.DeepL.com/Translator (free version)