Part Number: TRF37A73
Hi,
Q. Could you tell me the resistance value and tolerance of the internal pull-down resistor on the PWDN pin?
An NPN transistor is connected externally to switch between Hi and Lo.
However, the current design is 1.95V at Hi.
The specifications require 2V or more, so the pull-up resistor value (R525) must be considered.
Best regards,
Hiroshi