This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL052: TL052IP_ESD

Part Number: TL052
Other Parts Discussed in Thread: TL072H

Hi  TI Team,

TL052IP Qualification data is not available on TI.com. 

In the Qualification Summary, the results of ESD-HBM and CDM are described as "See data sheet".

However, the datasheet does not show the results of ESD.

Material name : TL052IP

(HBM:±●●V,CDM:±●●V) 

Best regards,

Sakamoto/TED

  • Hello Sakamoto-san,

    TL052 is one of the few older data sheet without ESD stated ratings. Is DIP package important for this application? If not then TL072H is recommended. 

    I did find ESD test results for TL052ACP , run in 1997 ; Results were HBM pass up to 1500V. MM pass 300V, CDM pass 2000V