Part Number: LMH2100
Hi team,
For ADC single-ended input, the ADC acquired voltage value should be VOUT = IDET* RTRANS + VREF. However, the VREF voltage is not told in the datasheet.

Look at the LMH2100 block diagram VREF should be the VREF voltage on the non-inverting input of the output amplifier.

However, in the following electrical table test conditions, VREF=0 and VREF=2.7V are seen.

Looking at the Pin Functions table REF pin type as the output type, it is not clear why the VREF value is not a fixed value. It can be 0V or 2.7 V.

Requesting your kind guidance here
Best Regards,
Amy Luo