Please check and inform can we use OP-Amp part no: OPA376AIDCKR by connecting +3.3V and -2.1V as working voltage as in specification, it was mentioned as 2.2-5.5V or ±1.1-2.75V.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please check and inform can we use OP-Amp part no: OPA376AIDCKR by connecting +3.3V and -2.1V as working voltage as in specification, it was mentioned as 2.2-5.5V or ±1.1-2.75V.
Hi Deepthi,
As Michael indicated, the delta voltage from the supply rails are within 5.5Vdc, so it complies with the OPA376 recommended operating conditions. Please make sure that 3.3Vdc and -2.1Vdc are properly decoupled and stiff voltage sources, and does not change the compliance voltage readily with a current load (regular LDOs should suffice).

If you have additional questions, please let us know.
Best,
Raymond