Other Parts Discussed in Thread: THS3001, THS6012
Hi Team TI, I'm noticing the noise simulation modelling for the THS3491 don't seem very accurate either. When I run the THS3491 on the bench with a gain of 2V/V R in = 1k and Rfb = 2k in a 150MHz bandwidth I get around 520uV. Doing the calculations the old fashioned way I get around 500uV which agrees pretty well with the bench measurements. (ie stray capacitance makes minimal effect). However when I run the simulation it erroneously tells me noise is only 425uV which is way off. Reducing Rf to 768 and Rin to 384 the simulated values are much closer. So it seems like the current noise coefficients could be off ? Any ideas, is it possible to hack the model so I can get correct results ? Also when do you plan to release the new and improved latest and greatest version? Thanks Steve