Hello,
I'm building a prototype with a single reverse bias (100V) photodiode (photoconductive mode) with a capacitance of 15pF.
I'd like to measure the amplitude (by sampling at around 100Mhz with 10bit ADC) laser pulse of 20ns of length with a quite high DC level (might be up to several mA) due to background light (so should be relatively low freq).
By making some calculation, the current due to the laser pulse could be very different from one setup to another one, typically from 1uA to 20mA.
The repetition rate of the laser pulse is very low, around 1Hz and the triggering of the sampling is done externally.
I thought about using a OPA847, any advice?
How can I cope with the quite high DC component ?
Thanks for your tips
Best regards,
PYB