Part Number: OPA858
Other Parts Discussed in Thread: OPA855
Hi Expert,
My customer is using OPA858 as a current source, but it couldn't work normally. could you help to give some advice? thanks.


Thanks.
BR
Chi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kai,
the input signal is 0.3 +- 0.1V,
the reason why customer want to use OPA858 is customer want to use one single OPA to cover all platform, OPA858 is used for TIA in optical module, this current bias is also used in optical project. the old solution is OPA855, now move to OPA858, we found that the OPA858 output current is different from OPA855. so ask your help to double check.
BR
Chi
Hi Kai,
thanks for your simulation result.
customer's use case,
input DC will be 0.9V, AC will be 0.3V+-0.1V
power supply is 3.3V and 5V, with 2 application scenario
output is at the node of BJT collector side. output current is 10mA
if this schematic is not stable, could you give some advice? thanks.
BR
Chi
Hello Chi,
I am closing this duplicate thread so responses can be focused onto the active thread.
Best,
Alec
Hi Alec,
sorry it is not a duplicated thread, my customer met a different application issue using one single OPA858. thanks.
BR
Chi
Hello Chi,
My apologies, my dashboard for viewing threads generated a copy of your thread. Please continue the discussion .
Best,
Alec