I am not sure if there is a way to use the Enable pin when using the output voltage boost circuit in Figure 76 of the datasheet.
The specs say that E/D com must be between V- and (V+)-5V. Since V+ on the bottom two amps can be at GND then is it true E/D com must be tied to (V-)?
How would I apply (V-)+5V to the center op amp's E/D pin when V- is ranging from -100V to 0V?
Thanks for the help.
David