Part Number: THS4521
Other Parts Discussed in Thread: ADC09QJ800,
Hello,
I am considering this part as driver to TI's ADC09QJ800.
In my application the signal will start from close to DC up to about (only) 120MHz.
(Yes - I know this ADC may seem an overkill but there are other factors involved also).
The ADC presents a 50 ohm input impedance to to common mode of 1.1V.
The datasheet of the THS4521 does not mention the output characteristics when driving a load of 50 ohm.
I will have many identical channels, so power dissipation and cost will also factor into the equation.
Could somebody comment on the choice of THS4521 in this application or suggest a better alternative.
2 and 3 Harmonic distortion are not critical for me.
Thanks