Other Parts Discussed in Thread: THS4552
Hi Team,
I am looking for a differential input & output amplifier.
goal is to design an active bandpass filter (fc~160-250kHz) after a mixer stage, which is differential out.
and it should drive a differential input PGA with 250 ohm input impedance.
- low noise ~5nV/sqrt(Hz)
- bandwidth ~10MHz minimum
- max Vin ~2Vpp
- Vcm ~1.2V common mode voltage
- drive at least 250 Ohm at output
- single supply 3-5V
- price <2 Euro
- 2 pieces (I and Q channel)
Looking forward to your recommendations!
BR,
Stefan